AXIS#.WS.TSTANDSTILL

Description

In Wake & Shake mode 1, a maximum current of AXIS#.WS.IMAX is applied to the AXIS#.MOTOR. AXIS#.WS.TSTANDSTILL defines a wait time, during which this maximum current is held, before detecting the commutation angle of the AXIS#.MOTOR. Longer times are useful for big inertia motors or heavy loads.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

100 to 20,000

Default Value

5000

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.WS.TSTANDSTILL

5013h

12h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6717

1

6717 (0x1a3d)

AXIS1.WS.TSTANDSTILL

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.WS.TSTANDSTILL

6717

Unsigned16

Read/Write

-